News Releases & Briefs
AUSTIN, Texas, Jan. 23, 2019 /PRNewswire/ -- Silicon Labs (NASDAQ: SLAB) expands its groundbreaking Wi-Fi portfolio of modules and transceivers, enabling developers to create end node products with best-in-class power efficiency, superior RF blocking performance and advanced security. Designed for the specific needs of IoT applications, the Wireless Gecko portfolio cuts Wi-Fi power consumption in half compared to competitive offerings, providing ideal Wi-Fi solutions for power-sensitive connected products, including battery-operated IP security cameras, point-of-sale scanners, asset trackers and personal medical devices.
![]()
"Our Wi-Fi portfolio enables IoT product designs that weren't possible until now," said Matt Johnson, Senior Vice President and General Manager of IoT products at Silicon Labs. "IoT developers now have a Wi-Fi solution that is truly optimized for their application requirements and addresses their major concerns around power, RF performance, size and security."
Half the power of existing Wi-Fi options: The combination of industry-leading transmit current (TX: 138 mA), receive current (RX: 48 mA) and sleep current (<40 µA) enables significant power-saving advantages for all IoT use cases. High throughput and fewer retransmissions help minimize power consumption by using less channel capacity.
State-of-the-art security: The Wi-Fi portfolio offers an array of built-in security features to protect IoT products from online and physical hacking, including secure boot with anti-rollback, secure link and efficient implementations of industry-standard encryption such as WPA3.
Superior RF blocking performance: Silicon Labs designed its Wi-Fi devices with excellent RF selectivity to block out adjacent channel noise and maintain throughput and connectivity in crowded RF environments such as smart homes with numerous connected devices.
Simple OS, dev tools and certification: Gecko OS, an optional, feature-packed IoT operating system, eases design complexity, allowing IoT developers to focus on their Wi-Fi applications. Developers can get started in minutes using comprehensive development tools and a wireless starter kit with embedded and Linux host drivers. The Wi-Fi modules are pre-certified for worldwide operation to reduce development time, effort and risk.
Silicon Labs' flexible Wi-Fi portfolio includes three device types:
- The WGM160P module – the portfolio's latest addition – expands design possibilities and offers an easier way to create cloud-connected IoT products by combining an onboard Gecko microcontroller, host support, integrated antenna, precertification, large memory (2 MB flash and 512K RAM), and extensive peripheral capabilities including Ethernet and capacitive touch.
- The WFM200 module is the smallest pre-certified Wi-Fi system-in-package (SiP) device with an integrated antenna, making it a perfect fit for space-constrained designs. The module also opens up new industrial and outdoor applications with 105 oC temperature support.
- The WF200 transceiver IC provides a cost-effective way to add Wi-Fi to existing high-volume designs, works well with a variety of hosts (ranging from 8-bit to Linux-class processors) and supports antenna diversity.
Pricing and Availability
Samples and production quantities of the WF200 transceiver in a 4 mm x 4 mm QFN32 package are available now. Samples of the WFM200 in a 6.5 mm x 6.5 mm SiP module are available now, and production quantities are planned for Q2 2019. Samples of the WGM160P in a PCB module are available now, and production quantities are planned for late February. Contact your local Silicon Labs sales representative or authorized distributor for WF200, WFM200 and WGM160P product pricing. For additional information, visit silabs.com/low-power-wi-fi.
Silicon Labs
Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software and solutions for a smarter, more connected world. Our award-winning technologies are shaping the future of the Internet of Things, Internet infrastructure, industrial automation, consumer and automotive markets. Our world-class engineering team creates products focused on performance, energy savings, connectivity and simplicity. silabs.com
Connect with Silicon Labs
Silicon Labs PR Contact: Dale Weisman +1-512-532-5871, dale.weisman@silabs.com
Follow Silicon Labs at news.silabs.com, at blog.silabs.com, on Twitter at twitter.com/siliconlabs, on LinkedIn at linkedin.com/company/siliconlabs and on Facebook at facebook.com/siliconlabs.
Cautionary Language
This press release may contain forward-looking statements based on Silicon Labs' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs' filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.
Note to editors: Silicon Labs, Silicon Laboratories, the "S" symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.
![]()
SOURCE Silicon Labs