News Briefs
-New PG22 microcontrollers enable high-volume, low-power consumer and industrial products-
AUSTIN, Texas – March 3, 2021 – Silicon Labs (NASDAQ: SLAB) announced the launch of the EFM32PG22 (PG22) 32-bit microcontroller unit (MCU), a low-cost, high-performance solution with an industry-leading combination of energy efficiency, performance and security. With easy-to-use, cost-efficient analog capabilities, the PG22 MCU is ideally suited for rapid development of consumer and industrial applications with demanding size constraints and low-power operation requirements.
“Market demand for high-volume, low-powered IoT products continues to grow at a rapid rate,” said Matt Saunders, vice president of IoT at Silicon Labs. “PG22 is an optimized 32-bit MCU, at a price point typically associated with the 8-bit MCU market, providing form factor and code compatibility with its wireless counterparts.”
PG22 offers best-in-class 32-bit MCU performance through a unique mix of product features including:
- Ultra-low-power – 27 µA/MHz Active and 1.1 µA EM2 with 8k RAM retention
- Arm® Cortex®-M33 core running at 76.8 MHz
- 64k / 128k / 256k / 512k Flash options with 32k RAM
- Compact package options – 5 mm x 5 mm QFN40 (26 GPIO) or 4 mm x 4 mm QFN32 (18 GPIO)
- Best-in-class device security including secure boot with Root of Trust and Secure Loader (RTSL)
- Wide range of peripherals such as 16-bit ADC, PDM, built-in sleep crystal and temp sensor
PG22 is pin- and software-compatible with the award winning EFR32xG22 wireless SoCs (BG22, MG22 and FG22), allowing designers to leverage a scalable embedded platform to simplify product development and help drive cost efficiency. Offering 100 percent form factor and code alignment with xG22 SoCs, developers can take advantage of application sharing and a drop-in upgrade path to Bluetooth Low Energy (LE), Zigbee or Proprietary (2.4 GHz) wireless connectivity.
Pricing and Availability
EFM32PG22 MCUs are currently available in 5 mm x 5 mm QFN40 and 4 mm x 4 mm QFN32 package options. PG22 MCUs provide cost-effective embedded processing with low volume pricing less than $1.00 (USD MSRP). The PG22 development kit, a small form factor prototype and development platform, is also available for purchase at $19.99 (USD MSRP). For additional information, visit silabs.com/pg22.
About Silicon Labs
Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software and solutions for a smarter, more connected world. Our award-winning technologies are shaping the future of the Internet of Things, Internet infrastructure, industrial automation, consumer and automotive markets. Our world-class engineering team creates products focused on performance, energy savings, connectivity and simplicity. silabs.com
Connect with Silicon Labs
Contact Silicon Labs PR team at pr@silabs.com.
Cautionary Language
This press release may contain forward-looking statements based on Silicon Labs’ current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs’ financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs’ filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise. Note to editors: Silicon Labs, Silicon Laboratories, the “S” symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.