News Releases & Briefs

New Silicon Labs Tiny Gecko MCUs Extend Battery Life for IoT Connected Devices

-- Ultra-Low-Power EFM32™ Microcontrollers Provide Secure, Feature-Rich Processing for Power-Sensitive Wireless Designs --

NUREMBERG, Germany (Embedded World) – Feb. 27, 2018 – Silicon Labs (NASDAQ: SLAB) has expanded its popular EFM32™ Tiny Gecko microcontroller (MCU) family to meet the needs of developers designing the next generation of secure, battery-powered connected devices for the Internet of Things (IoT). Silicon Labs’ new EFM32TG11 Tiny Gecko MCUs provide a cost-effective, ultra-low-power solution for connected devices requiring long battery life and no compromises in features or security. The Tiny Gecko 11 MCUs are ideal for smart meters, personal medical devices and home automation products with multiple sensors, local displays and touch controls. The new MCUs can be used in IoT designs as standalone microcontrollers or with network coprocessors, giving developers exceptional design flexibility.

The Tiny Gecko 11 MCUs are optimized for battery-powered applications offering cloud connectivity through wireless access points, gateways and concentrators. When paired with a Silicon Labs’ transceiver, SoC or module in many light-weight wireless applications, a Tiny Gecko 11 MCU can manage both the application code and wireless connectivity. When used with sophisticated protocols such as 802.11 b/g/n Wi-Fi®, the wireless system can be simplified by partitioning the Tiny Gecko 11 to solely manage the MCU application. The Tiny Gecko 11 MCUs include sufficient memory, sensor interfaces, peripherals, communication links and on-chip security to support both wireless use cases, as well as standalone MCU applications.

Based on an ARM® Cortex®-M0+ processor running at 48 MHz, the Tiny Gecko 11 MCUs provide ample processing power while maintaining very high energy efficiency. The MCUs combine low active current consumption (37 µA/MHz), fast wake-up times, a range of sleep modes (1.3 µA in deep sleep) and other architectural enhancements to enable secure, battery-powered IoT products requiring both high performance and low power consumption.

The Tiny Gecko 11 MCUs integrate an array of features that expand application possibilities:

  • Advanced capacitive sense controller with wake-on-touch capability for applications requiring touch interfaces
  • Low-energy sensor (LESENSE) interface for autonomous sensing in deep sleep modes
  • Patented 8x32 segment LCD controller, reducing power consumption by up to 40 percent
  • A CAN controller for industrial applications requiring wired connectivity  
  • Best-in-class hardware cryptography including AES, hash functionality (SHA), cyclical redundancy checks (CRC), an energy-efficient true random number generator (TRNG) and a security management unit (SMU), enabling fine-grained security for peripheral access

Software and pin-compatible with other EFM32 Gecko products, the new MCUs offer more flash memory (up to 128 kB) and RAM (up to 32 kB) than the previous Tiny Gecko generation, making it easier to develop feature-rich embedded applications supporting real-time operating systems (RTOS) such as Micrium OS.

Pricing and Availability

Samples and production quantities of the EFM32TG11 Tiny Gecko are available now in six package and size options, including an ultra-small 5 mm x 5 mm QFN32. Tiny Gecko 11 pricing begins at $1.65 (USD) in 10,000-unit quantities. The SLSTK3301A Starter Kit, available now at an introductory price of $89.00 (USD MSRP), enables developers to jumpstart evaluation and development of Tiny Gecko-based applications. The Tiny Gecko MCUs are supported by Silicon Labs’ Simplicity Studio development tools available to developers free of charge. To order Tiny Gecko 11 product samples and development kits, visit www.silabs.com/tg11.

Silicon Labs

Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software and solutions for a smarter, more connected world. Our award-winning technologies are shaping the future of the Internet of Things, Internet infrastructure, industrial automation, consumer and automotive markets. Our world-class engineering team creates products focused on performance, energy savings, connectivity and simplicity. www.silabs.com

Connect with Silicon Labs

Silicon Labs PR Contact: Dale Weisman +1-512-532-5871, dale.weisman@silabs.com

Follow Silicon Labs at http://news.silabs.com/, at http://blog.silabs.com/, on Twitter at http://twitter.com/siliconlabs, on LinkedIn at http://www.linkedin.com/company/siliconlabs and on Facebook at http://www.facebook.com/siliconlabs.

Cautionary Language

This press release may contain forward-looking statements based on Silicon Labs’ current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs’ financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs’ filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.

Note to editors: Silicon Labs, Silicon Laboratories, the “S” symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.

# # #