With our focus on energy efficiency, the Wonder Gecko kits give embedded designers access to the most energy-friendly ARM Cortex-M4 based MCU and the lowest standby power modes
AUSTIN, Texas--(BUSINESS WIRE)--Silicon Labs (Nasdaq: SLAB), a leader in high-performance, analog-intensive, mixed-signal ICs, today introduced development kits and application software demonstrations for the EFM32 Wonder Gecko microcontroller (MCU) family, which was developed by Energy Micro, recently acquired by Silicon Labs. The Wonder Gecko MCU line is based on the ARM® Cortex™-M4 processor core, which provides a full DSP instruction set and includes a hardware floating point unit (FPU) for faster computation performance. The development kits and software examples are designed to help embedded engineers leverage 32-bit digital signal control with the high-performance CPU and extremely low standby power modes.
“With our focus on energy efficiency, the Wonder Gecko kits give embedded designers access to the most energy-friendly ARM Cortex-M4 based MCU and the lowest standby power modes,” said Geir Førre, senior vice president and general manager of Silicon Labs’ microcontroller business. “The Wonder Gecko development kits and software library provide easy access to advanced signal processing functions and floating point performance. More and more instances of smart sensor and wireless applications benefit from effective analysis locally at the sensor node rather than transmitting large volumes of data over the network for remote processing.”
To speed up the design time, the EFM32 development kits include a built-in J-Link debugger and come with software examples using each kit’s built-in features:
These software demonstrations also enable designers to evaluate the differences between hard and soft floating-point operations and compiler optimization, as well as the CPU cycle count.
The example projects are coded using algorithms that are part of the Cortex Microcontroller Software Interface Standard (CMSIS) DSP function library, which includes complex FFT, finite impulse response (FIR) filters, matrix and vector operations, and statistical analysis. CMSIS provides a vendor-independent hardware abstraction layer for ARM Cortex-M processors.
Silicon Labs’ complimentary Simplicity Studio software suite includes all the necessary CMSIS, board support package (BSP) and documentation for the development kits including a Wonder Gecko white paper highlighting the 32-bit processing, DSP and FPU performance benefits of the EFM32 Wonder Gecko MCU family. The white paper also illustrates how the Wonder Gecko MCUs achieve high levels of 32-bit performance while delivering best-in-class energy efficiency.
Pricing and Availability
Silicon Labs’ EFM32 hardware evaluation platforms for the Wonder Gecko MCU family are available now. The EFM32WG-STK3800 starter kit, priced at $79 (USD), features an LCD segment display, light and touch sensors, and a USB interface to a host device. The full-featured EFM32WG-DK3850 development kit, priced at $349 (USD), includes a QVGA resistive-touch color display, audio connectors, a joystick, switches and a potentiometer for additional user controls. Both development kits provide advanced energy monitoring and real-time power profiling and are supported by the SEGGER J-Link debugger and the Simplicity Studio developer tools.
For more information and to order the EFM32 development kits for the Wonder Gecko MCU family, visit www.silabs.com/cortex-m4-kit.
Silicon Labs
Silicon Labs is an industry leader in the innovation of high-performance, analog-intensive, mixed-signal ICs. Developed by a world-class engineering team with unsurpassed expertise in mixed-signal design, Silicon Labs’ diverse portfolio of patented semiconductor solutions offers customers significant advantages in performance, size and power consumption. For more information about Silicon Labs, please visit www.silabs.com.
Cautionary Language
This press release may contain forward-looking statements based on Silicon Labs’ current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs’ financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs’ filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.
Note to editors: Silicon Laboratories, Silicon Labs, the “S” symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.
Follow Silicon Labs on Twitter at http://twitter.com/silabs and on Facebook at http://www.facebook.com/siliconlabs.
Explore Silicon Labs’ diverse product portfolio at www.silabs.com/parametric-search.
Silicon Labs
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com
or
Øyvind Borgan, +47 23 00 98 00
o.borgan@silabs.com