News Announcements
We welcome the release of the ZigBee IP specification because it gives semiconductor, software and system suppliers a single proven standard for developing and deploying low-power, cost-effective IP-based solutions for the Internet of Things
AUSTIN, Texas--(BUSINESS WIRE)--Silicon Labs (NASDAQ: SLAB), a leader in high-performance, analog-intensive, mixed-signal ICs, today announced that its Ember ZigBee solutions – silicon devices, software and development tools – have achieved Golden Unit certification from the ZigBee Alliance for the newly released ZigBee IP specification.
ZigBee IP is the first open standard for IPv6-based wireless mesh networking solutions, providing seamless, end-to-end Internet connectivity and a scalable architecture to control low-power devices. The new ZigBee IP specification adds network and security layers and an application framework to the IEEE 802.15.4 standard. It supports cost-effective, energy-efficient wireless mesh networks based on standard Internet protocols such as IPv6, 6LoWPAN, PANA, RPL, TCP, TLS and UDP. Ultimately, ZigBee IP will provide a standards-based foundation for Internet of Things (IoT) applications ranging from smart meters for the smart grid to in-home energy management systems to wireless sensor networks.
As one of the first to be certified by the ZigBee Alliance, Silicon Labs’ Ember ZigBee solutions, including EM35x wireless system-on-chip (SoC) devices, Ember ZigBee IP networking software and development tools, will serve as a preferred development platform for building and testing future connected products based on the ZigBee IP specification. The Golden Unit certification process instills confidence among developers and end users that all connected device products for the IoT from different vendors will interoperate seamlessly.
“We welcome the release of the ZigBee IP specification because it gives semiconductor, software and system suppliers a single proven standard for developing and deploying low-power, cost-effective IP-based solutions for the Internet of Things,” said Diwakar Vishakhadatta, vice president and general manager of Silicon Labs’ Embedded Systems group. “We look forward to continuing collaboration with the ZigBee Alliance and its members to promote ZigBee IP and implement the specification in a wide range of connected device products.”
About Ember ZigBee Solutions
Silicon Labs’ Ember ZigBee solutions include EM35x wireless devices, EmberZNet PRO software and development tools, providing a comprehensive, scalable platform for 2.4 GHz wireless mesh networking applications. The most widely used ZigBee platform for mesh networking applications, EM35x devices can be deployed as SoCs for cost-sensitive, low-power sensor networks and other simple connected devices or configured as network coprocessors (NCPs) for complex applications running on high-performance applications processors. The EM35x devices integrate a 2.4 GHz IEEE 802.15.4 wireless transceiver with an +8 dBm power amplifier, ARM® Cortex™-M3 processor, up to 192 kB flash memory and 12 kB RAM.
EM35x devices are tightly integrated with Silicon Labs’ EmberZNet PRO mesh networking protocol stack. Deployed in more wireless networking products than any other ZigBee stack, EmberZNet PRO software provides enhancements for robustness, scalability and ease-of-use even in larger networks and more challenging environments. The software stack is complemented by the Ember Desktop development environment, which reduces design time by providing sophisticated visualization and debugging tools and application templates for the ZigBee Smart Energy, Home Automation and Light Link profiles.
ZigBee: Control your world
ZigBee offers green and global wireless standards connecting the widest range of devices to work together intelligently and help you control your world. The ZigBee Alliance is an open, non-profit association of approximately 400 members driving development of innovative, reliable and easy-to-use ZigBee standards. The Alliance promotes worldwide adoption of ZigBee as the leading wirelessly networked, sensing and control standard for use in consumer, commercial and industrial areas. For more information, visit: www.ZigBee.org.
Silicon Labs
Silicon Labs is an industry leader in the innovation of high-performance, analog-intensive, mixed-signal ICs. Developed by a world-class engineering team with unsurpassed expertise in mixed-signal design, Silicon Labs’ diverse portfolio of patented semiconductor solutions offers customers significant advantages in performance, size and power consumption. For more information about Silicon Labs, please visit www.silabs.com.
Cautionary Language
This press release may contain forward-looking statements based on Silicon Labs’ current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs’ financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs’ filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.
Note to editors: Silicon Laboratories, Silicon Labs, the “S” symbol, the Silicon Laboratories logo, the Silicon Labs logo, Ember and EmberZNet are trademarks of Silicon Laboratories Inc. ZigBee is a trademark of the ZigBee Alliance. All other product names noted herein may be trademarks of their respective holders.
Follow Silicon Labs on Twitter at http://twitter.com/silabs and on Facebook at http://www.facebook.com/siliconlabs.
Explore Silicon Labs’ diverse product portfolio at www.silabs.com/parametric-search.
Contact:
Silicon Labs
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com