| Silicon Labs > Newsroom |
| News | ![]() |
|
||||||
Contact(s):
November 03 2008 Silicon Labs Introduces Industry's First Any-Rate, Any-Output Clock GeneratorSi5338 Simplifies Timing Architectures by Replacing Four Discrete PLLs
AUSTIN, Texas, November 03, 2008 -
Silicon
Laboratories Inc. (NASDAQ: SLAB), a leader in high-performance,
analog-intensive, mixed-signal ICs, today introduced a new family of
clock generators and buffers that provide the most frequency flexibility
in the industry. Based on Silicon Labs’
breakthrough MultiSynth technology, the Si5338 is capable of
synthesizing any frequency from 0.16 to 350 MHz and select frequencies
to 700 MHz on each of the device’s four
differential outputs, dramatically simplifying timing architectures by
replacing four discrete phase-locked loop (PLL) devices with a single
IC. Consistent with Silicon Labs’ timing
strategy of providing the most frequency flexible clock and oscillator
solutions in the industry, the Si5338 provides best-in-class performance
and integration while shortening design cycles for applications such as
next generation communications equipment, wireless base stations,
broadcast video, test and measurement and data acquisition.
At one picosecond rms random jitter typical, the Si5338 is able to
simultaneously generate low jitter clocks for a wide variety of ICs,
including processors, FPGAs, ASICs, memory and physical layer
transceivers. The device generates four differential or eight
single-ended outputs per device, eliminating the need for external clock
distribution buffers. In addition to frequency, each output clock is
independently configurable in terms of supply voltage (1.5V, 1.8V, 2.5V,
3.3V) and signal format (LVPECL, LVDS, CMOS, HCSL, SSTL, HSTL),
eliminating the need for external level translators and thereby reducing
BOM cost and complexity.
Historically, complex timing architectures have required multiple clock
generators and/or standalone crystal oscillators (XOs) to provide the
range of frequencies needed by the end application, often at the expense
of cost, design complexity and power. The any-rate, any-output
capability provided by the Si5338 dramatically simplifies timing
architectures by replacing fixed frequency clock generators, discrete
level translators and crystal oscillators with a single device,
minimizing cost and real estate and reducing power by 50 percent
compared to traditional solutions. To simplify board-level test, the
Si5338 includes a frequency margining feature that enables the frequency
of each output clock to be varied dynamically over the 0.16 to 350 MHz
range, eliminating discrete XOs and making it easier for hardware
designers to guarantee consistent, reliable system operation over
temperature and voltage.
For applications that do not require the programmability provided by the
Si5338, Silicon Labs is also introducing a broad portfolio of Si5334
pin-controlled clock generators. More than 70 Si5334 devices are
available for popular Ethernet, Fibre Channel, PCI Express, T1/E1,
broadcast video (HDTV) and SONET/SDH OC-3/12/48 applications. In
addition, Silicon Labs is introducing the Si5330 family of low-jitter,
low-skew clock buffers that support the widest range of output clock
formats in the industry. The new Si5330 flexible clock buffer produces 4
or 8 buffered copies of the input clock and is available in both
differential and single-ended versions.
“2008 has been a breakthrough year for Silicon
Labs timing products. We have added more than 100 devices to our overall
portfolio” said Dave Bresemann, vice president
of Silicon Labs. “The new product family of
any-rate, any-output clock generators and clock buffers complements
Silicon Labs’ existing products, providing the
industry’s broadest portfolio of timing
products and enabling Silicon Labs to provide customers a complete
clock-tree solution for next-generation designs.”
In addition to the new family of any-rate, any-output clock generators
and clock buffers, Silicon Labs offers a broad portfolio of frequency
flexible, low jitter any-rate, jitter attenuating clock multipliers and
low jitter silicon oscillators, XOs and VCXOs. These products use
optimized DSPLL® technology to shorten lead
times and deliver outstanding jitter performance for datacom, telecom,
wireless, broadcast video, test and measurement, and consumer markets.
Pricing and Availability
Packaged in a space-saving 24-lead 4x4mm QFN package, the Si5338, Si5334
and Si5330 are available now. Si5338 pricing starts at $9.31 in 10,000
piece quantities and is dependent on output frequency.
Silicon Laboratories Inc.
Silicon Laboratories is an industry leader in the innovation of
high-performance, analog-intensive, mixed-signal ICs. Developed by a
world-class engineering team with unsurpassed expertise in mixed-signal
design, Silicon Labs’ diverse portfolio of
highly integrated, easy-to-use products offers customers significant
advantages in performance, size and power consumption. These patented
solutions serve a broad set of markets and applications including
consumer, communications, computing, industrial and automotive.
Headquartered in Austin, TX, Silicon Labs is a global enterprise with
operations, sales and design activities worldwide. The company is
committed to contributing to our customers’
success by recruiting the highest quality talent to create
industry-changing innovations. For more information about Silicon Labs,
please visit www.silabs.com.
Cautionary Language
This press release may contain forward-looking statements based on
Silicon Laboratories’ current expectations.
These forward-looking statements involve risks and uncertainties. A
number of important factors could cause actual results to differ
materially from those in the forward-looking statements. For a
discussion of factors that could impact Silicon Laboratories' financial
results and cause actual results to differ materially from those in the
forward-looking statements, please refer to Silicon Laboratories’
filings with the SEC. Silicon Laboratories disclaims any intention or
obligation to update or revise any forward-looking statements, whether
as a result of new information, future events or otherwise.
Note to editors: DSPLL, Silicon Laboratories, Silicon Labs, the “S”
symbol, the Silicon Laboratories logo and the Silicon Labs logo are
trademarks of Silicon Laboratories Inc. All other product names noted
herein may be trademarks of their respective holders.
Related AssetsOther articles in News:
|