News 
Add Article to My Briefcase Print Friendly Version Convert to PDF Convert to RTF Related Assets Bookmark and Share

Contact(s):

Silicon Laboratories Inc.
Lindsey Starnes, +1 512-532-5349
lindsey.starnes@silabs.com


February 25 2008

Silicon Labs Introduces Industry's Lowest Voltage MCUs



--C8051F9xx Doubles Battery Life for Battery-Powered Products--

NUREMBERG, Germany & AUSTIN, Texas, February 25, 2008 - Silicon Laboratories Inc. (NASDAQ: SLAB), a leader in high-performance, analog-intensive, mixed-signal ICs, today announced the industrys first microcontrollers (MCUs) capable of operating down to 0.9 V, enabling portable devices to derive power from a single-cell battery for the first time at the Embedded World tradeshow in Nuremberg, Germany. The C8051F9xx familys novel 8-bit architecture with an integrated high-efficiency dc-dc boost converter, which can supply up to 65 mW of power for both internal MCU use and to drive other components, creates a true single-cell battery system solution. For products powered by user-replaceable batteries such as wireless sensor networks, smoke alarms, portable medical devices, remote controls, computer peripherals and portable audio devices, the C8051F9xx family enables smaller form factor products, longer battery life and lower overall system cost in both single- and dual-cell modes.

In many low-power applications, operating from 0.9 up to 3.6 V, the MCU is in sleep mode for the majority of the time, waking up periodically to capture data. The C8051F9xx utilizes innovative design techniques to deliver a typical sleep-mode current of less than 50 nA. The MCU can wake-up from its low power sleep mode with the CPU operating at 25 MIPS and ready to make an analog-to-digital converter (ADC) measurement within just two microseconds. This allows the MCU to spend a minimum amount of time performing measurements and algorithms. To save battery life in active mode, the C8051F9xxs power-efficient architecture yields an active-mode current as low as 170 µA/MHz.

The C8051F9xx family not only provides high performance while saving power but also unprecedented functional density in a small footprint. The C8051F9xx family is the first MCU to integrate 64 kB of Flash and 4 kB of RAM into a 4- x 4-mm package, providing customers with increased memory for typical applications such as data logging. The new low-voltage, low-power MCU family also integrates a 10-bit, 300-ksps analog-to-digital converter (ADC) with an internal fast wake-up voltage reference, a SmaRTClock timing module and multiple internal oscillator options to provide a true system-on-chip solution. This unprecedented integration is enabled by innovative design techniques manufactured in a standard low-power CMOS technology, resulting in fewer external components and reduced bill-of-materials cost for the customer.

Silicon Labs is revolutionizing the portable device market by enabling devices to operate from a single-cell battery, said Derrell Coker, vice president and general manager of Silicon Laboratories. Weve designed this industry-leading C8051F9xx MCU family with all customer concerns in mind to provide the lowest voltage operation and maximized power efficiency without sacrificing the mixed-signal functionality that differentiates Silicon Labs MCUs.

Silicon Labs best-in-class tools help speed design and accelerate market entry. A complete, low-cost professional development kit provides everything required to immediately begin system design including an integrated development environment (IDE), target board, cables and power supply. Also included in the kit is the Silicon Labs Power Battery Life Estimator, a GUI-based tool that provides details on typical battery discharge characteristics, as well as a user-editable spreadsheet allowing a designer to optimize the customers low-voltage, low-power MCU application. Designers can also begin risk-free evaluation using an inexpensive ToolStick daughter card and base adapter.

C8051F9xx Family

                     
                               
Device         Package         Flash         RAM
C8051F930-GQ        

32-pin

        64 kB         4 kB
C8051F930-GM        

32-pin

        64 kB         4 kB
C8051F931-GM        

24-pin

        64 kB         4 kB
C8051F920-GQ        

32-pin

        32 kB         4 kB
C8051F920-GM        

32-pin

        32 kB         4 kB
C8051F921-GM        

24-pin

       

32 kB

        4 kB

Pricing and Availability

The C8051F9xx family is available now in compact 24-pin, 4- x 4-mm QFN, 5- x 5-mm, 32-pin QFN and 7- x 7-mm, 32-pin LQFP packages. Pricing for the C8051F93x and C8051F92x families starts at $1.99 in quantities of 10K. Development kits are available for $99, and ToolStick daughter cards are available for $17.90. To purchase samples and development tools, please visit www.silabs.com/point9.

Silicon Laboratories Inc.

Silicon Laboratories is an industry leader in the innovation of high-performance, analog-intensive, mixed-signal ICs. Developed by a world-class engineering team with unsurpassed expertise in mixed-signal design, Silicon Labs diverse portfolio of highly integrated, easy-to-use products offers customers significant advantages in performance, size and power consumption. These patented solutions serve a broad set of markets and applications including consumer, communications, computing, industrial and automotive.

Headquartered in Austin, TX, Silicon Labs is a global enterprise with operations, sales and design activities worldwide. The company is committed to contributing to our customers success by recruiting the highest quality talent to create industry-changing innovations. For more information about Silicon Labs, please visit www.silabs.com.

Cautionary Language

This press release may contain forward-looking statements based on Silicon Laboratories current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Laboratories' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Laboratories filings with the SEC. Silicon Laboratories disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.

Note to editors: Silicon Laboratories, Silicon Labs, the S symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.

 


< back

Related Assets
 
Read this article in other languages: Other articles in News: