News Releases & Briefs

Silicon Labs Launches Timing Industry's Smallest, Lowest Jitter I2C-Programmable Crystal Oscillators

-- New small form factor XO/VCXOs simplify design in 400G/800G optical modules, deliver any-rate performance in industry's smallest footprint --

AUSTIN, Texas, Sep. 21, 2020 -- Silicon Labs (NASDAQ: SLAB) has introduced a new family of small form-factor, high-performance crystal oscillators (XOs) and voltage-controlled crystal oscillators (VCXOs) for applications that require low jitter and frequency-flexible clock synthesis.

The Si54x/6x Ultra Series XO/VCXOs deliver jitter performance as low as 80 femtoseconds (fs) for integer and fractional frequencies across the entire operating range, providing outstanding jitter margin for demanding applications including data center interconnect, optical transport, broadcast video and test/measurement. These new products are available with single, dual, quad and I2C-programmable frequency options in an industry-standard 2.5x3.2mm package footprint, making them ideal for space-constrained designs that require a mix of different frequencies.

Ideal for high bandwidth, high density line cards and small form factor optical modules

Increasing demand for network bandwidth and faster data rates are driving the need for higher speed 400/600/800G optical/Ethernet ports and higher density line cards.  With telco and data center applications accelerating 400G deployments, the optical module market is migrating from CFP designs to smaller form factor QSFP-DD, OSFP and CFP2 solutions to help ease the industry transition to higher bandwidth, higher density line cards. These applications require low jitter, highly reliable timing solutions to optimize system bit-error rates and ensure high system availability. 

Durable operation in a small footprint

The Si54x/6x are an ideal solution for 400/600/800G coherent optics and 56G/112G SerDes clocking in optical modules and line cards that require high performance in a small footprint.  The devices guarantee ±20 ppm operation over a 20-year operating life, making them ideal for long-life cycle applications.  All power supply filtering is integrated inside the device, eliminating discrete components that often consume as much PCB footprint as the XO itself.  Silicon Labs’ Si54x/6x are drop-in compatible with traditional oscillators while providing <2 week lead times for custom frequencies.

“Data center operators and telco networks are deploying lower-cost, smaller form factor optical modules for line-side and client-side applications, driving the need for space-optimized high-performance timing solutions,” said James Wilson, general manager of timing at Silicon Labs. “Unlike traditional solutions, which may require multiple oscillators to generate all required frequencies, the Si54x/Si56x is a single, unified solution that truly delivers any-rate performance in the industry’s smallest footprint.”

Silicon Labs’ expanding leadership in high-performance timing solutions

These new products further expand Silicon Labs’ industry-leading portfolio of high-performance XO/VCXOs, complementing a broad selection of options spanning general-purpose (800 fs), low-jitter (300 fs) and ultra-low jitter (80 fs) product families in 5x7mm, 3.2x5mm and 2.5x3.2mm package options. 

To help simplify oscillator selection and customization, Silicon Labs offers an array of simple web-based tools:

  • Part number utility enables designers to enter device specifications and generate an orderable part number in minutes
  • Oscillator phase noise look-up tool provides instant access to thousands of phase noise measurements, making it easy to view device phase noise and jitter performance across a wide range of operating frequencies
  • Cross-reference search utility helps customers find Silicon Labs second-source options for high-performance oscillators

Availability

Samples and production quantities of the Si54x/Si56x Ultra Series oscillators are available now.  For device evaluation, Silicon Labs offers the Si5xxUC-EVB universal evaluation board. For more information or to order samples and evaluation boards, visit www.silabs.com/ultra-series

About Silicon Labs

Silicon Labs is a leading provider of silicon, software and solutions for a smarter, more connected world. Our award-winning technologies are shaping the future of the Internet of Things, Internet infrastructure, industrial automation, consumer and automotive markets. Our world-class engineering team creates products focused on performance, energy savings, connectivity and simplicity.

Connect with Silicon Labs

Silicon Labs PR Conact: pr@silabs.com  

Cautionary Language

This press release may contain forward-looking statements based on Silicon Labs' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs' filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.

Note to editors: Silicon Labs, Silicon Laboratories, the "S" symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.