News Announcements
-
pdf (216 KB)Download Korean
-
pdf (212 KB)Download Simplified Chinese
-
pdf (272 KB)Download Traditional Chinese
We’re excited to help deliver the industry’s first low-power mbed platform, which will play a key role in accelerating the deployment of countless battery-powered IoT applications.
AUSTIN, Texas--(BUSINESS WIRE)--Silicon Labs (NASDAQ: SLAB), a leading provider of microcontroller, sensing and wireless connectivity solutions for the Internet of Things(IoT), today announced a collaboration with ARM to define and deliver the first power management application programming interfaces (API) for ARM® mbed™ platforms. Adding power management APIs to mbed will bring energy efficiency to standards-based solutions optimized for ultra-low-power, battery-operated connected devices. The new APIs will enable the mbed community of more than 100,000 registered developers to optimize their mbed-enabled ARM Cortex®-M architecture-based designs for the utmost energy efficiency and longer battery life.
In addition to enabling developers to manage processor and peripheral states, the mbed power management APIs are designed with real-world, low-energy application scenarios in mind. A new feature exposed by the APIs on Silicon Labs’ EFM32® Gecko microcontrollers (MCUs) automatically determines and enables the optimal sleep mode based on the MCU peripherals in use, which can dramatically reduce system-level energy consumption. Low-energy optimization is achieved by enabling I/O operations to be executed in the background and by allowing those operations to continue even while the MCU core is in sleep mode or during other processing tasks.
The automatic selection of the optimal sleep mode, combined with low-energy, autonomous MCU peripherals, enables developers to significantly reduce the energy consumption of their IoT applications with minimal effort. For example, energy profiles of an application updating a clock display every second on a memory LCD – a common use case for IoT devices – have shown a current consumption reduction from 1.03 mA to 0.100 mA.
“The new power management APIs for ARM mbed make it possible for developers to create applications that take advantage of the low-power features of ARM Cortex-M based microcontrollers,” said Zach Shelby, vice president, IoT business marketing, ARM. “This is an important step toward enabling full energy-awareness in IoT devices, and it is one of the key building blocks for mbed OS that is due for public release later this year.”
“As pioneers in low-energy processing solutions for the IoT, Silicon Labs and ARM have made enormous progress in defining and delivering the new power management APIs for mbed,” said Daniel Cooley, vice president and general manager of Silicon Labs’ MCU and wireless products. “We’re excited to help deliver the industry’s first low-power mbed platform, which will play a key role in accelerating the deployment of countless battery-powered IoT applications.”
Availability
Silicon Labs plans to provide mbed-enabled EFM32 Gecko starter kits in April 2015. Silicon Labs’ initial platforms supporting mbed will include the Wonder Gecko, Leopard Gecko, Giant Gecko and Zero Gecko starter kits. Developers with existing EFM32 kits will be able to mbed-enable their hardware through a simple software update. For more information about Silicon Labs’ mbed platforms, please visit www.silabs.com/mbed.
Silicon Labs
Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software and system solutions for the Internet of Things, Internet infrastructure, industrial automation, consumer and automotive markets. We solve the electronics industry’s toughest problems, providing customers with significant advantages in performance, energy savings, connectivity and design simplicity. Backed by our world-class engineering teams with unsurpassed software and mixed-signal design expertise, Silicon Labs empowers developers with the tools and technologies they need to advance quickly and easily from initial idea to final product. www.silabs.com
Cautionary Language
This press release may contain forward-looking statements based on Silicon Labs’ current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs’ financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs’ filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.
Note to editors: Silicon Labs, Silicon Laboratories, the “S” symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.
Follow Silicon Labs at http://news.silabs.com/, at http://blog.silabs.com/, on Twitter at http://twitter.com/siliconlabs and on Facebook at http://www.facebook.com/siliconlabs.
Explore Silicon Labs’ diverse product portfolio at www.silabs.com/parametric-search.
Contact:
Silicon Labs
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com