News Announcements
-
pdf (292 KB)Download Japanese
-
pdf (282 KB)Download Korean
-
pdf (352 KB)Download Traditional Chinese
-
pdf (256 KB)Download Simplified Chinese
Embedded development in the IoT age is an increasingly complex endeavor, especially when developing ultra-low-power, wireless-enabled connected devices
NUREMBERG, Germany--(BUSINESS WIRE)--Silicon Labs (NASDAQ: SLAB), a leading provider of microcontroller, wireless connectivity, analog and sensor solutions for the Internet of Things (IoT), today introduced the next generation of Simplicity Studio™, the industry’s first integrated MCU/wireless development environment enabling concurrent MCU and RF design for a wide range of IoT applications. This new software release inherits the best features of the original Simplicity Studio platform and adds support for Silicon Labs’ new 8-bit EFM8 MCU family, new EZR32 sub-GHz wireless MCUs and EM35xx Ember ZigBee® wireless SoCs – the most widely used 2.4 GHz connectivity solution in the 802.15.4 mesh networking market.
Simplicity Studio simplifies the process of developing IoT applications by providing MCU and wireless developers with one-click access to everything they need to complete their projects, from initial concept to final product, in a unified software environment. Simplicity Studio includes an Eclipse-based integrated development environment (IDE), graphical configuration tools, energy profiling tools, network analysis tools, demos, software examples, documentation, technical support and community forums. All of these integrated features combine to make embedded development simple and productive for IoT developers.
Simplicity Studio offers built-in intelligence to automatically detect the connected 8-bit or 32-bit MCU or wireless IC, graphically configure the device, and show supported configuration options to help developers get their projects up and running in minutes. Simplicity Studio is a contextually aware development environment that provides developers with product information that is relevant to their project. Integrated real-time energy profiling and network packet analyzer tools also enable developers to create robust networks and energy-efficient wireless nodes and to enhance energy consumption for optimal battery life and size.
Concurrent MCU and wireless design within the same development environment helps customers save time and effort by eliminating context switching during the embedded design process. Embedded developers can use the integrated Simplicity Studio IDE for rapid application development of target applications based on EZR32 wireless MCUs, Ember ZigBee wireless SoCs and 8/32-bit MCUs. The IDE supports enhanced usability features such as full integration of the wireless embedded software framework, intelligent code completion, and compatibility with other value-added extensions available from the Eclipse ecosystem.
Silicon Labs also provides the Keil® PK51 build tools for 8-bit 8051 MCUs at no charge ($2,500 savings for customers). GNU Compiler Collection (GCC) build tools are included for EFM32 Gecko MCU designs while EZR32 designs use the IAR EWARM compiler with Silicon Labs’ wireless stacks. Developers who prefer to use their own IDE can launch Keil µVision or IAR Embedded Workbench through Simplicity Studio by configuring their “preferred IDE.”
“Embedded development in the IoT age is an increasingly complex endeavor, especially when developing ultra-low-power, wireless-enabled connected devices,” said Daniel Cooley, vice president of MCU and wireless products at Silicon Labs. “Fractured tool chains also place a growing training and overhead burden on embedded developers, particularly for IoT projects that require MCU, wireless and sensor components. Our new version of Simplicity Studio dramatically simplifies the design process by enabling IoT developers to concurrently work with MCUs and wireless devices in the same unified environment.”
The Simplicity Studio development platform is available to developers at no charge and can be downloaded by visiting www.silabs.com/simplicity-studio.
Simplicity Studio Platform Highlights
- NEW: Concurrent MCU and wireless design capabilities
- NEW: Support for the new EFM8 Bee 8-bit MCU family
- NEW: Support for the new EZR32 wireless MCU family
- NEW: Packet Trace analyzer for real time inspection of network traffic
- COMING SOON: Support for the EM35xx Ember ZigBee wireless SoC family available by late Q1 2015
- COMING SOON: Integrated AppBuilder tool for rapid development of ZigBee applications available by late Q1 2015
- Eclipse-based integrated development environment (IDE) for both 8- and 32-bit MCUs
- Auto-configuration for connected MCU, simplifying embedded development
- Energy profiler to analyze power consumption and optimize code
- Configurator tool to quickly configure MCUs and wireless MCUs and generate C-code for pinout, peripherals and mode transitions
- One-click access to demos, software examples, data sheets, application notes, technical support and community forums
- Capacitive Sense Profiler tool enabling developers to view the library’s measured performance on C8051F97x and C8051F99x MCU families, providing real-time output of measured counts as well as button/slider event detection
- Mac® OS X and Linux support in addition to existing Windows® OS support
Silicon Labs
Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software and system solutions for the Internet of Things, Internet infrastructure, industrial automation, consumer and automotive markets. We solve the electronics industry’s toughest problems, providing customers with significant advantages in performance, energy savings, connectivity and design simplicity. Backed by our world-class engineering teams with unsurpassed software and mixed-signal design expertise, Silicon Labs empowers developers with the tools and technologies they need to advance quickly and easily from initial idea to final product. www.silabs.com
Cautionary Language
This press release may contain forward-looking statements based on Silicon Labs’ current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs’ financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs’ filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.
Note to editors: Simplicity Studio, EFM32, Silicon Labs, Silicon Laboratories, the “S” symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.
Follow Silicon Labs at http://news.silabs.com/, at http://blog.silabs.com/, on Twitter at http://twitter.com/siliconlabs and on Facebook at http://www.facebook.com/siliconlabs.
Explore Silicon Labs’ diverse product portfolio at www.silabs.com/parametric-search.
Contact:
Silicon Labs
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com