News Announcements
-
-
pdf (230 KB)Download Simplified Chinese
-
pdf (283 KB)Download Traditional Chinese
-
pdf (361 KB)Download Japanese
Silicon Labs is the only UV index sensor vendor that offers a broad portfolio of energy-friendly MCUs, wireless MCUs and transceivers, and an array of other sensors that can be combined into system solutions for the fast-growing wearables market.
AUSTIN, Texas--(BUSINESS WIRE)--Silicon Labs (NASDAQ: SLAB), a leader in high-performance, analog-intensive, mixed-signal ICs, today introduced the industry’s first single-chip digital ultraviolet (UV) index sensor ICs designed to track UV sun exposure, heart/pulse rate and blood oximetry and provide proximity/gesture control for smartphone and wearable computing products. The latest additions to Silicon Labs’ optical sensor family, the Si1132 and Si114x sensor ICs are ideal for activity-tracking wrist and arm bands, smart watches and smartphone handsets. In addition to enabling UV index sensing, the devices also provide ambient light and infrared (IR) proximity sensing capabilities for health and fitness applications.
The demand for UV sensing in consumer electronics is rising as developers seek to differentiate wearable and handset products with new features that help protect people from harmful UV light exposure. UV tracking is helpful for those with elevated risks of sunburn or concerns about excessive sun exposure. UV sensor-equipped products can measure cumulative UV exposure and alert end users before they have reached unhealthy exposure levels while exercising outdoors. Standardized by the World Health Organization (WHO), the digital UV index is linearly related to the intensity of sunlight and is weighted according to the Erythemal Action Spectrum developed by the International Commission on Illumination (CIE). This weighting provides a standardized measure of our skin’s response to different sunlight wavelengths including UVB and UVA.
Conventional UV sensors combine UV-sensitive photodiodes with an external microcontroller (MCU), analog-to-digital converter (ADC) and signal processing firmware. Silicon Labs is the first to combine all of this functionality into a single-chip solution offered in an exceptionally small 2 mm x 2 mm package that helps reduce the design’s footprint and bill of material (BOM) cost. The UV sensor family includes the following devices:
- Si1132 UV index and ambient light sensor with an industry-standard I2C interface to read digital UV index values
- Si1145/46/47 UV and IR proximity/ambient light sensors offering a choice of one, two or three integrated LED drivers with 15 selectable drive levels for gesture detection.
When combined with an accelerometer, the Si1132 and Si114x sensors enable developers to implement sleep tracking in wearable applications. In addition, the sensors’ ability to measure both infrared and visible light levels enhances the control of LCD backlighting in mixed light source environments. The result is an inexpensive yet effective means of adjusting backlighting to ease eyestrain and reduce power without distracting the end user.
The Si114x sensors’ LED drivers enable implementation of reflective heart rate and blood oximetry measurement capabilities for health and fitness trackers, as well as touchless interfaces that support end-user control from a distance. Offering two and three infrared LED drivers respectively, the Si1146 and Si1147 sensors enable advanced motion and gesture sensing. The Si1146 enables motion sensing and touchless control in the z- and x-axis, and the Si1147 adds a third axis to enable 3-dimensional motion sensing. Both sensors provide reflectance measurements that can be post-processed to determine gestures.
The Si1132 and Si114x sensors offer excellent performance under a wide dynamic range of light sources including direct sunlight. The robust sensing architecture also includes an ambient light sensor capable of sensing light levels up to 128 kLux. The photodiode response and associated digital conversion circuitry provide excellent immunity to artificial light flicker noise and natural light flutter noise.
The UV index sensors’ ultra-low-power architecture enables thinner wearable designs with smaller batteries and extends battery life with as little as 1.2 µA average current for once-per-second UV measurements. The sensors also offer greater sensitivity and sensing range at significantly lower power levels than competitive offerings. The high IR sensor sensitivity provides significantly longer battery life in motion sensing/gesture applications through the use of a single 25.6 µs IR-LED on-time while enabling up to 50 cm sensing range. Dynamic adjustment of LED currents further minimizes power consumption.
“Wearable designs require highly integrated, small-footprint and low-power sensing solutions, and we’re meeting this need with the industry’s first single-chip digital UV index sensors that also provide ambient light and IR sensing capabilities for innovative health and fitness applications,” said Mark Thompson, vice president and general manager of Silicon Labs’ Access, Power and Sensor products. “Silicon Labs is the only UV index sensor vendor that offers a broad portfolio of energy-friendly MCUs, wireless MCUs and transceivers, and an array of other sensors that can be combined into system solutions for the fast-growing wearables market.”
Silicon Labs provides wearable developers with comprehensive hardware and software tools to simplify testing, characterization, prototyping and software development. The UVIrSlider2EK UV/IR evaluation kit provides an advanced development platform for Silicon Labs’ optical sensors. Controlled by an ultra-low-power C8051F800 MCU, the UVIrSlider2EK connects the Si1146 sensor to two IR-LEDs, enabling UV index measurements, advanced 2D/2-axis touchless gesture detection and object proximity detection. The IrSlider2EK is pre-configured with firmware that displays the five-level consumer UV strength index on five LEDs. Demo software provides a GUI with the full UV index and an IR slider demo that demonstrates left/right/pause gesture detection using eight visible LEDs. In addition, Silicon Labs provides example software source code for ambient light, proximity and gesture detection algorithms.
Pricing and Availability
Samples and production quantities of Silicon Labs’ Si1132 and Si114x UV sensors are available now in a 10-pin 2 mm x 2 mm QFN package. The Si1132 sensor is priced at $1.10 in 10,000-unit quantities, and 10K pricing for the Si114x sensors begins at $1.32 (all prices USD). The UVIrSlider2EK evaluation kit is priced at $50 (USD MSRP).
For additional Si1132 and Si114x UV index sensor information and to order samples and development tools, please visit www.silabs.com/opticalsensors.
Silicon Labs
Silicon Labs is an industry leader in the innovation of high-performance, analog-intensive, mixed-signal ICs. Developed by a world-class engineering team with unsurpassed expertise in mixed-signal design, Silicon Labs’ diverse portfolio of patented semiconductor solutions offers customers significant advantages in performance, size and power consumption. For more information about Silicon Labs, please visit www.silabs.com.
Cautionary Language
This press release may contain forward-looking statements based on Silicon Labs’ current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs’ financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs’ filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.
Note to editors: Silicon Laboratories, Silicon Labs, the “S” symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.
Follow Silicon Labs on Twitter at http://twitter.com/silabs and on Facebook at http://www.facebook.com/siliconlabs.
Explore Silicon Labs’ diverse product portfolio at www.silabs.com/parametric-search.
Contact:
Silicon Labs
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com